Verifying Frequency of LPC4357

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Verifying Frequency of LPC4357

697 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sal Ammoniac on Tue Mar 24 19:17:47 MST 2015
The LPC4357 has a somewhat complicated clock generation and distribution system. Is there a straightforward way to determine if the CPU is actually running at 204 MHz? I think I have all of the clock CGU/CCU registers programmed correctly for 204 MHz, but I'd like an independent way to verify it's actually running at that speed.
标签 (1)
0 项奖励
回复
1 回复

686 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Mar 24 20:33:00 MST 2015
Hi Sal,
You can divide PLL out(Core Clock) by two and send it to CLKOUT pin for measurement.
0 项奖励
回复