Values of Reserved Bits in CMPA/CFPA Registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Values of Reserved Bits in CMPA/CFPA Registers

Jump to solution
2,712 Views
LucianA
Contributor I

Hello!

I have a question regarding how to set Reserved bits in the following registers
DCFG_CC_SOCU_NS_PIN (bits 14:10, and

DCFG_CC_SOCU_NS_DFLT (bits 15:10, 8).

In User Manual, for SECURE_BOOT_CFG (page 153), PRINCE_BASE_ADDR (page 154) etc

it is specified that Reserved Bits should be filled with zeros.

Is that also mandatory for Reserved Bits in DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_NS_DFLT?

Thank you!

0 Kudos
Reply
1 Solution
2,639 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI LucianA 

If you don't want to enforce UUID checking, please leave these bits as default (0)

Hope this helps,

Jun Zhang

View solution in original post

0 Kudos
Reply
4 Replies
2,699 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI LucianA 

To resolve your problem, please let me know,

- your chip part number

- document screenshot of where you concerned about.

Thanks for your cooperation,

Jun Zhang

0 Kudos
Reply
2,693 Views
LucianA
Contributor I

Hi Jennie,

According to "LPC55S6x_LPC55S2x_LPC552x Protected Flash Region v1.3.xlsx"

DCFG_CC_SOCU_NS_PIN and DCFG_CC_SOCU_NS_DFLT registers have the same format for all those families.

However, I'm particularly interested for LPC5528 device.
It's a must to write zeros in the Reserved Bits marked in red in the attached picture (DCFG_CC_SOCU_NS_PIN[14:10] and DCFG_CC_SOCU_NS_PIN[8])  ?

Thank you!

0 Kudos
Reply
2,640 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI LucianA 

If you don't want to enforce UUID checking, please leave these bits as default (0)

Hope this helps,

Jun Zhang

0 Kudos
Reply
2,632 Views
LucianA
Contributor I

Thanks Jennie,

I will keep all reserved bits on default values (zeros).

 

0 Kudos
Reply