Content originally posted in LPCWare by floreste on Wed Jun 18 04:07:40 MST 2014
Hello,
I am having some troubles using your debug probe and your IDE to evaluate a board, and I would like some help regarding my troubles.
I am using the LPC433x-Xplorer (that works well regarding to the quick start guide whose steps I have checked) and my troubles are with the LPC-Link 2 debug probe. I have read that it was quite easy to handle (plug and play) when used with the LPCXpresso IDE. I am new to this software too, and may have wrongly configured it.
So when I launch the Debug ‘LPC4330_Xplorer_Blinky’ [Debug] from the quickstartup menu, I get this error (cf screenshot).
I have tried to install the drivers for the debug probe several times manually, but it keeps coming as an HMI in the device manager (cf screenshot) is that normal?
Finally, I have tried to run the DFU programmer to boot the debug probe, but it did not work better, and normally I should not use this software with LPCXpresso IDE.
So, I hope you can help me, I’m looking forward for your answer
Regards
Florent ESTEVENY