Updating firmware using UART for LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Updating firmware using UART for LPC1768

1,026 次查看
ashokrabadiya
Contributor I

Hello,

 

I am flashing my code through Flash Magic over UART0, just wanted to know whether I can Flash it over other UART ? 

 

If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3 ?

 

Thanks in Advance

标签 (1)
0 项奖励
回复
1 回复

929 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Ashok Rabadiya,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3?
-- No, I'm afraid the UART3 is unavailable

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复