Unexpected DMA Behaviour with LPC1778 Two

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unexpected DMA Behaviour with LPC1778 Two

609 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Jan 14 22:18:35 MST 2013
I'm using LPCXpresso 4.3 to debug (because I am not convinced of v5 stability yet) on WinXP Prof SP3 (32 bit)
LPC1778 Custom PCB

I forgot to set the EnableDMA bit in the FIFO register when I set up my uart (Uart0)
Then I setup the RX DMA channel as if I had.

The surprising thing is that the RX DMA is working as expected -- i.e. received characters can be seen in the DMA
buffer.

Can anyone explain this or othwerwise shed light on the issue.

See also my thread "Unexpected DMA Behaviour with LPC1778".

Mike
标签 (1)
0 项奖励
回复
0 回复数