Unable to 'download and debug' for OM13067 demo board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to 'download and debug' for OM13067 demo board

1,444 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by afiqahlaa on Mon Aug 03 20:09:11 MST 2015
Hi,

I had bought a motor control demo board for PMSM motor (OM13067) which work together with LPC1549 board.
http://www.nxp.com/demoboard/OM13067.html

I am facing a problem to 'download and debug' the code given by the developer. So basically I just follow step by step given in the manual. Connected the boards and motor, open the code using IAR IDE. But when come to the step where I need to 'download and debug' I was unable to do that.

The question is do I need any debugger probe to download and debug the provided code? Since for the demo board package only provided:

- LPCXpresso Motor Control Board, rev. B
- LPCXpresso LPC1549 Board
- Permanent Magne motor.

Thank you in advance!
标签 (1)
0 项奖励
回复
2 回复数

1,436 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by afiqahlaa on Tue Aug 04 00:56:38 MST 2015
Thank you for the reply and I am so sorry for the wrong doing I did. Will read the post.
0 项奖励
回复

1,436 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 04 00:33:22 MST 2015
Please see the answer posted in the other thread you posted on this:

https://www.lpcware.com/content/forum/debug-lpc1549-using-iar-ide#comment-1147171

[ And please don't create multiple threads for the same issue!! ]

Regards,
LPCXpresso Support
0 项奖励
回复