Uart Buad Rate Error of LPC55xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uart Buad Rate Error of LPC55xx

1,352件の閲覧回数
rahul_4
Contributor II

Hi,

UART Baud Rate error and is not defined in the datasheet. Can you please tell me, what is the Uart buad rate error in LPC55xx series?

Thanks,

Rahul

0 件の賞賛
返信
3 返答(返信)

1,325件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @rahul_4 

I'm not able to understand completely what are you refering to.

Is it possible for you to provide a more detailed explanation to look for the correct answer please?

Best Regards, Miguel.

0 件の賞賛
返信

1,309件の閲覧回数
rahul_4
Contributor II

Hi Miguel,

If the selected UART Baud Rate is 9600, what is the error percentage in the output? Is it within +-1% or +-3%?

For +-1% it will be -> 9504 to 9696 baud rate

Thanks,
Rahul

0 件の賞賛
返信

1,289件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @rahul_4 

There isn't a specification about a deviation on the baudrates generated for the uart. The baudrate deviation could be affected by the precision of the clock.

Best Regards, Miguel.

0 件の賞賛
返信