Uart Buad Rate Error of LPC55xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uart Buad Rate Error of LPC55xx

1,506 Views
rahul_4
Contributor II

Hi,

UART Baud Rate error and is not defined in the datasheet. Can you please tell me, what is the Uart buad rate error in LPC55xx series?

Thanks,

Rahul

0 Kudos
Reply
3 Replies

1,479 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @rahul_4 

I'm not able to understand completely what are you refering to.

Is it possible for you to provide a more detailed explanation to look for the correct answer please?

Best Regards, Miguel.

0 Kudos
Reply

1,463 Views
rahul_4
Contributor II

Hi Miguel,

If the selected UART Baud Rate is 9600, what is the error percentage in the output? Is it within +-1% or +-3%?

For +-1% it will be -> 9504 to 9696 baud rate

Thanks,
Rahul

0 Kudos
Reply

1,443 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @rahul_4 

There isn't a specification about a deviation on the baudrates generated for the uart. The baudrate deviation could be affected by the precision of the clock.

Best Regards, Miguel.

0 Kudos
Reply