USB_VENDOR class BULK_IN transfer got 0 size data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB_VENDOR class BULK_IN transfer got 0 size data

475 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by albert.ke on Sun Dec 08 22:41:57 MST 2013
I am working on NXP1768 and want to use Vender defined class of USB bulk in transfer.

The using scenario are Host send command by Endpoint 0 and the NXP1768 need to send data in to HOST with command USB_WriteEP() by Bulk endpoint 3 which I defined after the command.

After USB_WriteEP(), the Host receive no data.

The following is my descriptor definitions.
============================================================================
/* USB Standard Device Descriptor */

const U8 USB_DeviceDescriptor[] = {
  USB_DEVICE_DESC_SIZE,              /* bLength */
  USB_DEVICE_DESCRIPTOR_TYPE,        /* bDescriptorType */
  WBVAL(0x0200), /* 2.00 */          /* bcdUSB */
  0x00,                              /* bDeviceClass */
  0x00,                              /* bDeviceSubClass */
  0x00,                              /* bDeviceProtocol */
  USB_MAX_PACKET0,                   /* bMaxPacketSize0 */
  WBVAL(USB_VENDOR_ID), /* idVendor */
  WBVAL(USB_PRODUCT_ID), /* idProduct */
  WBVAL(USB_RELEASE_NO), /* 1.00 */ /* bcdDevice */
  0x01,                              /* iManufacturer */
  0x02,                              /* iProduct */
  0x00,                              /* iSerialNumber */
  0x01                               /* bNumConfigurations: one possible configuration*/
};

/* USB Configuration Descriptor */
/*   All Descriptors (Configuration, Interface, Endpoint, Class, Vendor) */
const U8 USB_ConfigDescriptor[] = {
/* Configuration 1 */
  USB_CONFIGUARTION_DESC_SIZE,       /* bLength */
  USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType */
  WBVAL(                             /* wTotalLength */
    1*USB_CONFIGUARTION_DESC_SIZE +
    1*USB_INTERFACE_DESC_SIZE     +
    2*USB_ENDPOINT_DESC_SIZE
  ),
  0x01,                              /* bNumInterfaces */
  0x01,                              /* bConfigurationValue: 0x01 is used to select this configuration */
  0x00,                              /* iConfiguration: no string to describe this configuration */
  USB_CONFIG_BUS_POWERED /*|*/       /* bmAttributes */
/*USB_CONFIG_REMOTE_WAKEUP*/,
  USB_CONFIG_POWER_MA(100),          /* bMaxPower, device power consumption is 100 mA */

/* Interface 0, Alternate Setting 0, vendor Class */
  USB_INTERFACE_DESC_SIZE,           /* bLength */
  USB_INTERFACE_DESCRIPTOR_TYPE,     /* bDescriptorType */
  0x00,                              /* bInterfaceNumber */
  0x00,                              /* bAlternateSetting */
  0x02,                              /* bNumEndpoints */
  USB_DEVICE_CLASS_VENDOR_SPECIFIC,  /* bInterfaceClass */
  USB_DEVICE_SUBCLASS_VENDOR_SPECIFIC,/* bInterfaceSubClass */
  USB_DEVICE_PROTOCOL_VENDOR_SPECIFIC,/* bInterfaceProtocol */
  0x00,                              /* iInterface */

/* Endpoint, EP3 Bulk IN */
  USB_ENDPOINT_DESC_SIZE,            /* bLength */
  USB_ENDPOINT_DESCRIPTOR_TYPE,      /* bDescriptorType */
  USB_ENDPOINT_IN(3),                /* bEndpointAddress */
  USB_ENDPOINT_TYPE_BULK,            /* bmAttributes */
  WBVAL(0x0040),                     /* wMaxPacketSize */
  0x00,                              /* bInterval: ignore for Bulk transfer */

/* Endpoint, EP3 Bulk OUT */
  USB_ENDPOINT_DESC_SIZE,            /* bLength */
  USB_ENDPOINT_DESCRIPTOR_TYPE,      /* bDescriptorType */
  USB_ENDPOINT_OUT(3),               /* bEndpointAddress */
  USB_ENDPOINT_TYPE_BULK,            /* bmAttributes */
  WBVAL(0x0040),                     /* wMaxPacketSize */
  0x00,                              /* bInterval: ignore for Bulk transfer */
/* Terminator */
  0                                  /* bLength */
};
============================================================================
I can use the same Host program in Atmel chip and it work well.
Can anyone give some suggestions about this issue?


Thanks
Albert

标签 (1)
0 项奖励
0 回复数