USB ISP mode without external crystal?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB ISP mode without external crystal?

1,182 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dmaroto on Thu Aug 13 04:28:03 MST 2015
I am trying to use the USB ISP mode to program an application for the first time and the micro (LPC1547) does not seem to enter into USB ISP mode.

I have checked the voltages and states of ISP_0 and ISP_1 during power up and all seems to be as it should.

I did see this note in section 5.4 of the user manual:

Remark: In USB ISP mode, an external 12 MHz crystal is required  to communicate with the external storage device. (I did not consider the chip Flash as "external" when designing the circuit).

Can the LPC1547 actually start in USB ISP mode without an external clock?

Thank you for your help.
标签 (1)
0 项奖励
回复
1 回复

1,145 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Aug 13 05:13:01 MST 2015

Quote: Dmaroto
Can the LPC1547 actually start in USB ISP mode without an external clock?



No  :((
0 项奖励
回复