UAC 5.1 channel configuration for lpcxpresso55s28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UAC 5.1 channel configuration for lpcxpresso55s28

238件の閲覧回数
PatrickLai
Contributor I

Hi,

I am testing the UAC on lpcxpresso55s28 using the sample code dev_audio_speaker_freertos from the SDK SDK_25_03_00_LPCXpresso55S28. The default 2 channel UAC is ok. But when I try to configure it to 5.1-channel following the document "Implementation of 5.1-channel Audio Solution on LPC55xx", it seems not working. Because I click the "configure" button for the UAC speaker, there is no window pops up like below. Please help to check it. Thanks!

PatrickLai_0-1751962180445.png

 

0 件の賞賛
返信
1 返信

230件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @PatrickLai 

Did you test it with SDK 2.14.0? This AN is based on the SDK 2.14.0.

Harry_Zhang_0-1752035108531.png

BR

Harry

0 件の賞賛
返信