U8glib: LCD and OLED graphics library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U8glib: LCD and OLED graphics library

2,525 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by olikraus on Fri Oct 04 15:54:20 MST 2013
Hi All

The graphics library U8glib has been ported to Cortex-M0 controller. The ARM version of U8glib includes examples for NXP LPC1114 and NXP LPC1226 controller.

Project URL: http://code.google.com/p/u8glib/

[list]
  [*] Low RAM usage
  [*] Support for many LCD/OLED controller (SSD1306, SSD1325, ST7565, ST7920, UC1610, UC1701, ...)
[/list]

Oliver
Labels (1)
0 Kudos
Reply
2 Replies

1,827 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by olikraus on Wed Jul 09 21:50:09 MST 2014
Yes, but need to update the hardware abstraction layer for the 176x controller. In the 1114 example, locate file common/u8g_arm.c. This file needs to be updated. Also see INSTALL.TXT.

Another user has provided also this: http://blog.bastelhalde.de/?p=759

Oliver
0 Kudos
Reply

1,827 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dandumit on Wed Jul 09 07:43:46 MST 2014
Hello Oliver,
could it be used for 176x ?
Kind REgards,
Daniel
0 Kudos
Reply