Setting of DEBUG_LOCK_EN on LPC55S69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting of DEBUG_LOCK_EN on LPC55S69

1,594件の閲覧回数
__marvin__
Contributor II

Hi,

I would like to disable the debug- as well as the programming- (SWD) interfaces on our custom LPC55S69 board  in order to secure our IP.

While reading the DEBUG_FEATURES and DEBUG_FEATURES_DP returns as expected, reading DEBUG_LOCK_EN resulted in 0x5, which means all write accesses to the debug and programming registers are permitted and ignored.

I was wondering, where the write lock is set to 0x5 in the examples. I couldn't find the line.

Hope you can help me with this.

 

Thanks for your help and all the best,
marvin

0 件の賞賛
返信
4 返答(返信)

1,573件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Marvin,

So you would like to set 0xA to the register? This means that you enable write access to security registers.

I also read value when starting a new project and I also read 0x5 value. I am going to contact internal team to see if they have some feedback about this.

FelipeGarcia_0-1623948685415.png

Best regards,

Felipe

0 件の賞賛
返信

1,569件の閲覧回数
__marvin__
Contributor II

Hi Felipe,

thanks for verifying this.
If there should be a response, please let me know.

All the best,
marvin

0 件の賞賛
返信

1,555件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Marvin,

I have received confirmation from internal team. Please check it below.

After POR, the related six registers (CPU0_DEBUG_FEATURES,CPU1_DEBUG_FEATURES…) will be configured based on the PFR data in the CFPA DCFG_CC_SOCU_NS_PIN and  DCFG_CC_SOCU_NS_DFLT (0x9de20 – 0x9de27), and CMPA DCFG_CC_SOCU_PIN and DCFG_CC_SOCU_DFLT (0x9e410 – 0x9e41b), and then the ROM will set DEBUG_LOCK_EN to 0x5.

You can refer to AN13037(LPC55Sxx Debug Authentication) for details.

Best regards,

Felipe

1,545件の閲覧回数
__marvin__
Contributor II

Thank you so much! This really helped me a lot.

0 件の賞賛
返信