Sending a byte over UART0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sending a byte over UART0

1,626 次查看
nabeelfattah
Contributor II

Hello,

I am using LPC4330 chip and LPCXpresso IDE for programming.

My target is sending and receiving data from UART. I write below code for sending 1 Byte of data as primary test but I can not see any things on the oscilloscope.

Can someone tell me where is the problem? I use UART example for writing this code.

Please, if you know how to use UART for sending and receiving data from UART let me know.

The code:

#ifdef __USE_CMSIS
#include "LPC43xx.h"
#endif

#include <cr_section_macros.h>

#if defined (__MULTICORE_MASTER_SLAVE_M0APP) | defined (__MULTICORE_MASTER_SLAVE_M0SUB)
#include "cr_start_m0.h"
#endif

// TODO: insert other include files here
#include "Physical_interface.h"
#include "board.h"
#include "uLED_functions.h"
unsigned char smiley_PWM[90*90];

// TODO: insert other definitions and declarations here
LPC_USART_T *pUART=LPC_USART0_BASE;
#define LPC_UART LPC_USART0
//#define LPC_UART LPC_UART1
#define UARTx_IRQn USART0_IRQn
#define UARTx_IRQHandler UART0_IRQHandler
#define _GPDMA_CONN_UART_Tx GPDMA_CONN_UART0_Tx
#define _GPDMA_CONN_UART_Rx GPDMA_CONN_UART0_Rx

/* Ring buffer size */
#define UART_RB_SIZE 256

/* Transmit and receive ring buffers */
STATIC RINGBUFF_T txring, rxring;

FlagStatus exitflag;
uint8_t buffer[10];
int ret = 0;
int len;


/* Transmit and receive buffers */
static uint8_t rxbuff[UART_RB_SIZE], txbuff[UART_RB_SIZE];

static uint8_t uartABStart[] = "Starting UART Auto-Baud - Press 'A' or 'a'! \n\r";
static uint8_t uartABComplete[] = "UART Auto-Baudrate synchronized! \n\r";

/* Uart Polling variables and functions declaration */
static uint8_t uartPolling_menu1[] = "Hello NXP Semiconductors \r\n";
static uint8_t uartPolling_menu2[] = "UART polling mode demo \r\n";
static uint8_t uartPolling_menu3[] = "\r\nUART demo terminated!";
static uint8_t uartPolling_menu4[] = "\r\nPress number 1-3 to choose UART running mode:\r\n"
"\t 1: Polling Mode \r\n"
"\t 2: Interrupt Mode \r\n"
"\t 3: DMA Mode \r\n";
static uint8_t uartPolling_menu5[] = "\r\nPolling mode is running now! Please press \'c\' and choose another mode \r\n";

/* Uart Interrupt variables and functions declaration */
static uint8_t uart_interrupt_menu[] =
"UART Interrupt mode demo ! \r\nPress '1' to '4' to display 4 menus \r\nPress 'x'to exit UART interrupt mode \r\n";
static uint8_t uart_interrupt_menu1[] = "UART interrupt menu 1 \r\n";
static uint8_t uart_interrupt_menu2[] = "UART interrupt menu 2 \r\n";
static uint8_t uart_interrupt_menu3[] = "UART interrupt menu 3 \r\n";
static uint8_t uart_interrupt_menu4[] = "UART interrupt menu 4 \r\n";
/* static uint8_t rxUartIntBuf[1]; */

#define DMA_TIMEOUT 0xA000000

/* DMA variables and functions declaration */
static uint8_t dmaChannelNumTx, dmaChannelNumRx;
static uint8_t uartDMA_menu[] = "Hello NXP Semiconductors (DMA mode)\r\n"
"UART DMA mode demo ! Please type 'hello NXP' to return\r\n";

static volatile uint32_t channelTC; /* Terminal Counter flag for Channel */
static volatile uint32_t channelTCErr;
static FunctionalState isDMATx = ENABLE;


/*****************************************************************************
* Private functions
****************************************************************************/

/* Initialize DMA for UART, enable DMA controller and enable DMA interrupt */
static void App_DMA_Init(void)
{
/* Initialize GPDMA controller */
Chip_GPDMA_Init(LPC_GPDMA);
/* Setting GPDMA interrupt */
NVIC_DisableIRQ(DMA_IRQn);
NVIC_SetPriority(DMA_IRQn, ((0x01 << 3) | 0x01));
NVIC_EnableIRQ(DMA_IRQn);
}

/* DeInitialize DMA for UART, free transfer channels and disable DMA interrupt */
static void App_DMA_DeInit(void)
{
Chip_GPDMA_Stop(LPC_GPDMA, dmaChannelNumTx);
Chip_GPDMA_Stop(LPC_GPDMA, dmaChannelNumRx);
NVIC_DisableIRQ(DMA_IRQn);
}

/* DMA routine for example_uart */
static void App_DMA_Test(void)
{
uint8_t receiveBuffer[16];

App_DMA_Init();
dmaChannelNumTx = Chip_GPDMA_GetFreeChannel(LPC_GPDMA, _GPDMA_CONN_UART_Tx);

isDMATx = ENABLE;
channelTC = channelTCErr = 0;
Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumTx,
(uint32_t) &uartDMA_menu[0],
_GPDMA_CONN_UART_Tx,
GPDMA_TRANSFERTYPE_M2P_CONTROLLER_DMA,
sizeof(uartDMA_menu));
while (!channelTC) {}

dmaChannelNumRx = Chip_GPDMA_GetFreeChannel(LPC_GPDMA, _GPDMA_CONN_UART_Rx);
isDMATx = DISABLE;
channelTC = channelTCErr = 0;
Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumRx,
_GPDMA_CONN_UART_Rx,
(uint32_t) &receiveBuffer[0],
GPDMA_TRANSFERTYPE_P2M_CONTROLLER_DMA,
10);
while (!channelTC) {}

isDMATx = ENABLE;
channelTC = channelTCErr = 0;
Chip_GPDMA_Transfer(LPC_GPDMA, dmaChannelNumTx,
(uint32_t) &receiveBuffer[0],
_GPDMA_CONN_UART_Tx,
GPDMA_TRANSFERTYPE_M2P_CONTROLLER_DMA,
10);
while (!channelTC) {}

App_DMA_DeInit();
}

/* Print Welcome Screen Menu subroutine by Interrupt mode */
static void Print_Menu_Interrupt(LPC_USART_T *UARTx)
{
uint32_t tmp;
uint8_t *pDat;

tmp = sizeof(uart_interrupt_menu);
pDat = (uint8_t *) &uart_interrupt_menu[0];
Chip_UART_SendRB(UARTx, &txring, pDat, tmp);
}

/* Initialize Interrupt for UART */
static void App_Interrupt_Init(void)
{
/* Enable UART Rx & line status interrupts */
/*
* Do not enable transmit interrupt here, since it is handled by
* UART_Send() function, just to reset Tx Interrupt state for the
* first time
*/
Chip_UART_IntEnable(LPC_UART, (UART_IER_RBRINT | UART_IER_RLSINT));

/* Before using the ring buffers, initialize them using the ring
buffer init function */
RingBuffer_Init(&rxring, rxbuff, 1, UART_RB_SIZE);
RingBuffer_Init(&txring, txbuff, 1, UART_RB_SIZE);

/* Enable Interrupt for UART channel */
/* Priority = 1 */
NVIC_SetPriority(UARTx_IRQn, 1);
/* Enable Interrupt for UART channel */
NVIC_EnableIRQ(UARTx_IRQn);
}

/* DeInitialize Interrupt for UART */
static void App_Interrupt_DeInit(void)
{
/* Disable UART Rx & line status interrupts */
Chip_UART_IntDisable(LPC_UART, (UART_IER_RBRINT | UART_IER_RLSINT));

/* Disable Interrupt for UART channel */
NVIC_DisableIRQ(UARTx_IRQn);
}

/* Interrupt routine for example_uart */
static void App_Interrupt_Test(void)
{
uint8_t isExit = 0, userInput;
int len;
App_Interrupt_Init();

/* Print out uart interrupt menu */
Print_Menu_Interrupt(LPC_UART);

while (!isExit) {
len = 0;
while (len == 0) {
len = Chip_UART_ReadRB(LPC_UART, &rxring, &userInput, 1);
}
if (userInput == '1') {
Chip_UART_SendRB(LPC_UART, &txring, (uint8_t *) &uart_interrupt_menu1[0], sizeof(uart_interrupt_menu1));
}
else if (userInput == '2') {
Chip_UART_SendRB(LPC_UART, &txring, (uint8_t *) &uart_interrupt_menu2[0], sizeof(uart_interrupt_menu2));
}
else if (userInput == '3') {
Chip_UART_SendRB(LPC_UART, &txring, (uint8_t *) &uart_interrupt_menu3[0], sizeof(uart_interrupt_menu3));
}
else if (userInput == '4') {
Chip_UART_SendRB(LPC_UART, &txring, (uint8_t *) &uart_interrupt_menu4[0], sizeof(uart_interrupt_menu4));
}
else if (( userInput == 'x') || ( userInput == 'X') ) {
isExit = 1;
}
}

App_Interrupt_DeInit();
}

/* Print Welcome menu by Polling mode */
static void Print_Menu_Polling(void)
{
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu1, sizeof(uartPolling_menu1));
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu2, sizeof(uartPolling_menu2));
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu5, sizeof(uartPolling_menu5));
}

/*****************************************************************************
* Public functions
****************************************************************************/

/**
* @brief GPDMA interrupt handler sub-routine
* @return Nothing
*/
void DMA_IRQHandler(void)
{
uint8_t dmaChannelNum;
if (isDMATx) {
dmaChannelNum = dmaChannelNumTx;
}
else {
dmaChannelNum = dmaChannelNumRx;
}
if (Chip_GPDMA_Interrupt(LPC_GPDMA, dmaChannelNum) == SUCCESS) {
channelTC++;
}
else {
channelTCErr++;
}
}

/**
* @brief UART interrupt handler sub-routine
* @return Nothing
*/
void UARTx_IRQHandler(void)
{
Chip_UART_IRQRBHandler(LPC_UART, &rxring, &txring);
}

/**
* @brief Main UART program body
* @return Always returns -1
*/


int main(void) {

// Start M0APP slave processor
unsigned int i=0;
unsigned char xx=0x55;
unsigned int gg=1;
uint8_t buffer[10];

//LPC_USART_T *pUART=LPC_USART0_BASE;

#if defined (__MULTICORE_MASTER_SLAVE_M0APP)
cr_start_m0(SLAVE_M0APP,&__core_m0app_START__);
#endif

// Start M0SUB slave processor
#if defined (__MULTICORE_MASTER_SLAVE_M0SUB)
cr_start_m0(SLAVE_M0SUB,&__core_m0sub_START__);
#endif


Board_UART_Init(LPC_UART);
/* Enable UART Transmit */
Chip_UART_TXEnable(LPC_UART);


Chip_UART_Init(LPC_UART);
Chip_UART_SetBaud(LPC_UART, 115200);
Chip_UART_ConfigData(LPC_UART, UART_LCR_WLEN8 | UART_LCR_SBS_1BIT); /* Default 8-N-1 */

/* Enable UART Transmit */
Chip_UART_TXEnable(LPC_UART);

Chip_UART_Init(LPC_UART);
//Chip_UART_Init(pUART);
Chip_UART_SetBaud(LPC_UART,9600);
//Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT, 5, 1);
Chip_UART_Send(LPC_UART,buffer,10);

// TODO: insert code here
Chip_SetupCoreClock(CLKIN_CRYSTAL, MAX_CLOCK_FREQ, true);
SystemCoreClockUpdate();


// Enter an infinite loop, just incrementing a counter
for (i=0;i<8101;i++)
{
smiley_PWM[i]=simily2[i]*Opt_nuer[i];
}
while(1) {

/* Reset FIFOs, Enable FIFOs and DMA mode in UART */
Chip_UART_SetupFIFOS(LPC_UART, (UART_FCR_FIFO_EN | UART_FCR_RX_RS |
UART_FCR_TX_RS | UART_FCR_DMAMODE_SEL | UART_FCR_TRG_LEV0));

/* Enable UART End of Auto baudrate & Auto baudrate timeout interrupts */
Chip_UART_IntEnable(LPC_UART, (UART_IER_ABEOINT | UART_IER_ABTOINT));

/* preemption = 1, sub-priority = 1 */
NVIC_SetPriority(UARTx_IRQn, 1);
/* Enable Interrupt for UART0 channel */
NVIC_EnableIRQ(UARTx_IRQn);

/* Send UART Autobaud completed message */
Chip_UART_SendBlocking(LPC_UART, uartABStart, sizeof(uartABStart));

/* ---------------------- Auto baud rate section ----------------------- */
/* Start auto baudrate mode */
Chip_UART_ABCmd(LPC_UART, UART_ACR_MODE0, true, ENABLE);

/* Loop until auto baudrate mode complete */
while (Chip_UART_GetABEOStatus(LPC_UART) == RESET) {}

/* Send UART Autobaud completed message */
Chip_UART_SendBlocking(LPC_UART, uartABComplete, sizeof(uartABComplete));

/* Disable UART Interrupt */
NVIC_DisableIRQ(UARTx_IRQn);

/* Print welcome screen */
Print_Menu_Polling();

exitflag = RESET;
/* Read some data from the buffer */
while (exitflag == RESET) {
len = 0;
while (len == 0) {
len = Chip_UART_Read(LPC_UART, buffer, 1);
}
if (buffer[0] == 27) {
/* ESC key, set exit flag */
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu3, sizeof(uartPolling_menu3));
ret = -1;
exitflag = SET;
}
else if (buffer[0] == 'c') {
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu4, sizeof(uartPolling_menu4));
len = 0;
while (len == 0) {
len = Chip_UART_Read(LPC_UART, buffer, sizeof(buffer));
if ((buffer[0] != '1') && (buffer[0] != '2') && (buffer[0] != '3')) {
len = 0;
}
}
switch (buffer[0]) {
case '1': /* Polling Mode */
Chip_UART_SendBlocking(LPC_UART, uartPolling_menu5, sizeof(uartPolling_menu5));
break;

case '2': /* Interrupt Mode */
ret = 2;
/* Exitflag = SET; */
App_Interrupt_Test();
Print_Menu_Polling();
break;

case '3': /* DMA mode */
ret = 3;
App_DMA_Test();
Print_Menu_Polling();
break;
}
}
}


/* Wait for current transmission complete - THR must be empty */
while (Chip_UART_CheckBusy(LPC_UART) == SET) {}

/* DeInitialize UART0 peripheral */
//Chip_UART_DeInit(LPC_UART);

Chip_UART_Send(pUART,&xx,1);
delay(1000);

}
return 0 ;
}

0 项奖励
回复
1 回复

1,139 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Nabeel Fattah,

  You can refer to this post:

https://community.nxp.com/message/853121?commentID=853121#comment-853121 

  This is the test result:

pastedImage_1.png

  You also can refer to the lpcopen code for LPCXpresso IDE, I have test it,it can printf out the data.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复