SPI Slave select of LPC54102

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Slave select of LPC54102

1,128 Views
tejaljagdale
Contributor I

Hello,

I am using LPC54102  and I am trying to run example code from LPCopen library.  If I run example code as it is on may hardware it is working fine, but I if make changes in SSEL pin i.e Slave select pin it is not working as expected.

Please help me related same.

0 Kudos
Reply
2 Replies

939 Views
tejaljagdale
Contributor I

Thanks Victor, I'll try with SDK.

Tejal

0 Kudos
Reply

939 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Tejal,

Are you using the example periph_spi_sm_int from the LPCopen or another one? 

What pin are you selecting when you make the change for the Slave select pin? 

The LPC54102 board has SDK, so I recommend you to use this instead of the LPCOpen, this because SDK is the newest software so all the new updates and bug fixes will come for SDK only. You can download it from here

I'll be waiting for your answer to continue with this problem!

Have a great day, 

Victor.

0 Kudos
Reply