SCT - PWM 200K Hz 100puse,not use interupt to STOP。

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCT - PWM 200K Hz 100puse,not use interupt to STOP。

1,582件の閲覧回数
yansinli
Contributor III

SCT0產生一個200KHz AB pulse輸出波形,當user設定100次pulse(200KHz AB) 後,自動將SCT0關掉. (不用中斷去關掉SCT0,因為隨MCU的負載量變大,會導致來不及去關掉SCT0,導致額外多輸出101次的波形)

SCT0有甚麼方法可去完成這個應用?不使用中斷。

------------------------------------------------------------------------------------

SCT0  ouput PWM 200K AB , user set 100 pulse (200K AB),auto halt SCT0.( not use interupt close SCT0, because MCU High loading,Interupt will delay and not imediately halt SCT0. lead to ouput 101 pulse).

what sct have other way to do this applicaion? not use interupt.

MY mcu LPC1519

タグ(1)
0 件の賞賛
返信
1 返信

1,443件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,
非常感谢使用NXP产品,很高兴为你提供技术支持!
已在https://community.nxp.com/thread/517699 中回复,请查看。

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信