SB 2.1 (1B) Flash out of date CFPA page

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SB 2.1 (1B) Flash out of date CFPA page

跳至解决方案
6,448 次查看
mohammed_aitben
Contributor II

Hi all,

I am working on LPC55S69-EVK with 1B chip.

I can't update my image with SB 2.1.

1- Loading CFPA image, i have this status error : KstatusFlashOutOfDateCFPAPage

2- I have Other issue with my device, Actually can't erase flash. The device is locked. Is there any way to unlock it ?

Please any help. Thanks in advance.

Best regards

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

Your version looks OK (version 0x 00 00 00 01)

When you want to update CFPA then you need to increment CFPA version at least +1

Please use any hex editor for CFPA generation/modification. All registers are described in UM->Protected_Flash_Region.xlsx

I do not see any attached file.

Regards,

Tomas

在原帖中查看解决方案

18 回复数
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

SB file config looks OK.

Could you share with me CMPA and CFPA page? Read through debugger when you are in SECURE state (not possible to use read-memory command). Hopefully you did not disabled already debug ports.

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Hello,

I don't know which ports you are talking about, but I have nothing disabled.

I can't use read-memory in blhost tools  !

Could you please tell me how can read through debugger ?

0 项奖励
回复
6,073 次查看
mohammed_aitben
Contributor II

Hello TomasVoda‌,

I took a new device, this one it's not  locked :smileyhappy:  

1- But i get always flash out of date cfpa page How can i set correctly my CFPA page ?

     > blhost -p COM12 read-memory 0X9DE18 0x4
         Ping responded in 1 attempt(s)
         Inject command 'read-memory'
         Successful response to command 'read-memory'
         55 00 00 00
         (1/1)100% Completed!
         Successful generic response to command 'read-memory'
         Response status = 0 (0x0) Success.
         Response word 1 = 4 (0x4)
         Read 4 of 4 bytes.


2- How we can avoid locking device ?

Thanks 

Best regards

0 项奖励
回复
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

2) When updating CMPA please do not write hash field.

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Hash field ? Are you talking about RKTH ? 

0 项奖励
回复
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

NO, about SHA-256 digest at the end of page.

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Sorry, it's not clear for me. In the application notes they don't talk about SHA-256 at the end of CMPA ? which level are you talking about ?

Can't send you my CFPA binary ! 

0 项奖励
回复
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

About which AppNote you are talking? Where did you download demo package CFPA?

SHA-256 digest is written at the end CMPA when you are at the end of development and you will change your security state to SECURE. After that it is not possible to change CMPA content and ISP commands are limited.

Please see Protected_flash_region.xlsx file attached to UM where you can see all registers in CMPA/CFPA.

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

I am talking about AN12283 app notes.

I download package demo from from community : https://community.nxp.com/message/1266918?commentID=1266918#comment-1266918 

below my CFPA binary file. 

You said that my CFPA looks OK ! but when i write CFPA 0X9DE00 i get always : Flash out of date CFPA PAGE !

CFPA.png

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Hey TomasVoda

I edited my CFPA file and I moved 0x9DE18 @ to 0x01 value.

But still can't update my CFPA PAGE into device !

Any help !

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Hey TomasVoda 

The CFPA PAGE update it works.

Thanks 

0 项奖励
回复
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

CFPA version is based at address  0x9de04 -> blhost -p COM12 read-memory 0X9DE04 0x4 (keep in mind endianness)

When you want to update CFPA than version of new CFPA has to be higher then previous version.

How do you want to update CFPA? I expect you use blhost -p COM12 write-memory 0X9DE00 new_cfpa.bin

Be sure that in new_cfpa.bin which is 512B file is at address 0x4 incremented version register.

Also keep in mind for proper security setting we have one way changing possibilities for some registers in CFPA.

Ensure the secureFwVersion in new CFPA must be >= existing secureFwVersion

Ensure the nsFwVersion in new CFPA must be >= existing nsFwVersion

Ensure the vendorUsage in new CFPA must be >= existing vendorUsage

 

Ensure that the imageKeyRevoke must be >= existing imageKeyRevoke

Note the imagekeyRevoke are treated like OTP, the version increasing flow, (0, 1, 3, 7, etc)

 

Ensure that the rotkhRevoke must be >= existing rotkhRevoke

Note the rotkhRevoke are treated like OTP, the version increasing flow, (0, 1, 3, 7, etc)

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Hi @Tomas

Thank you for answers.

Reading my CFPA at 0x4 : 

>blhost -p COM12 read-memory 0X9DE04 0x4
   Ping responded in 1 attempt(s)
   Inject command 'read-memory'
   Successful response to command 'read-memory'
   01 00 00 00
   (1/1)100% Completed!
   Successful generic response to command 'read-memory'
   Response status = 0 (0x0) Success.
   Response word 1 = 4 (0x4)
   Read 4 of 4 bytes.

I have one CFPA.bin file i download from demo package which is 1Ko ! see attached file !

How can i generate a new CFPA file ?

Thanks  

0 项奖励
回复
6,075 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

Your version looks OK (version 0x 00 00 00 01)

When you want to update CFPA then you need to increment CFPA version at least +1

Please use any hex editor for CFPA generation/modification. All registers are described in UM->Protected_Flash_Region.xlsx

I do not see any attached file.

Regards,

Tomas

6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hi Mohammed,

1) Please see thread: LPC55S69 Secure Boot Failing  and check your CFPA register Version at 0x4

2) How is locked your device? When you move to deployment state there is not way how to unlock.

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

Thanks for answer.
I already saw this thread, they don't explain how they fixed CFPA error.

1) How can i check my CFPA PAGE at 0x4 ?

2) I can't eras flash memory, So i guess it's locked : 

>blhost -p COM 12 flash-erase-all

       Response status = 10001 (0x2711) Command disallowed when security is enabled.

If that's the case, I don't know how it's locked, i was just trying to update my image through SB 2.1.


>12 get-property 17
     Ping responded in 1 attempt(s)
     Inject command 'get-property'
     Response status = 0 (0x0) Success.
     Response word 1 = -1019428036 (0xc33cc33c)
     Security State = SECURE

Thanks

0 项奖励
回复
6,074 次查看
tomas_voda
NXP Employee
NXP Employee

Hello Mohammed,

CFPA page has at offset 0x4 Version register. Each time when you load new CFPA page Version has to be incremented for loading new CFPA page.

Could you please send me .bd file configuration?

Security state is locked when you write CMPA hash.

When you move into SECURE state then there are limited ISP commands (flash-erase-all is not allowed).

Regards,

Tomas

0 项奖励
回复
6,074 次查看
mohammed_aitben
Contributor II

OK

Below my CommandFile.bd configuration :

options {
flags = 0x8; // 0x4 //encrypted
buildNumber = 0x1;
productVersion = "1.00.00";
componentVersion = "1.00.00";
secureBinaryVersion = "2.1";
}

sources {
mainImage = "\signed_led_blinky.bin";
}

section (0) {
erase 0x0000..0x40000;
load mainImage > 0x0;
//call mainImage;
//reset;
}

0 项奖励
回复