Hello Team,
I have to do the i2c program in my custom board which having lpc11e36 microcontroller.
Below I attached my present code please review and give the comments.
Mainly tell me about board library files, where i will get this board library files.
Regards,
Kamalesh.C
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello kamalesh
For LPC11xx, please refer to LPCOpen Software for LPC11XX | NXP Semiconductors
You can check the available examples "LPCOpen for LPC11E68", I2C demo is included.
Hope this will help you.
Have a nice day,
Jun Zhang
Hello Zhang,
In this software examples, There is lpc11U6x.c examples. I have uploaded this example. But no response.
Can i use the lpc11u6x series example for my lpc11e36 microcontroller?
I tried UART Program, this itself is not happening. But my UART Program is working well.
Regards,
Kamalesh
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi kamalesh,
I don't have LPC11e36 board to test. But please try lpcopen for LPC11u37 board. Can it work for you?
Best Regards,
Jun Zhang
Hello zhang,
Actually I tried the uart example for my board. This itself is not working. How this i2c will work??
I have uart example for my board, it is working fine. so it is based on the library file or board file. i have the i2c driver and uart driver file. but my example is not working. I given my program for your reference.
I tried ethernet examples also with my board. it is working super fine. but for this i2c, it is giving trouble now.
What can i do for this i2c now?
Feel free to ask any question.
Best Regards,
Kamalesh.C
 
					
				
		
 ZhangJennie
		
			ZhangJennie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi kamalesh
Could you please confirm, Does the default lpcopen for LPC11u37 board I2C demo project (without any change) work on your lpcopen for LPC11E36 board? I need to know if the problem is related with the PCB design.
Thanks,
Jun Zhang
Hello ZhangJennie,
I tried the i2c program from the lpcopen examples of LPC11u37 in my board. But unfortunately, it is not working in my board.
I tried the normal uart examples from that same lpcopen examples, it is not working for me. This is the one I explained in my previous post.
If my explanation is not in understandable manner, feel free to ask again.
Regards,
Kamalesh
 Joey_z
		
			Joey_z
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		hi kamalesh ,
I used LPC11U37 to do some IIC experiments. I used the LPC11U37 development board to run the“ nxp_lpcxpresso_11u37h_periph_i2c” program in LPCopen. Through this program, the LPC11U37 development board was configured as a master. Then the LPC55S69 development board was used to run the “lpcxpresso55s69_i2c_polling_b2b_slave” program as a slave.
The operation of the LPC11U37 master in the experiment is shown in the figure below.
In the figure, 0x48 is the slave address set in the“ lpcxpresso55s69_i2c_polling_b2b_slave ”program running on the LPC55S69. By debugging this program, *buf = (uint8_t)base->SLVDAT in the I2C_SlaveReadBlocking function can be used to view the data written from the master. At the same time, the transmission data that can be viewed through the logic analyzer is shown in the figure.
Note: After each read and write operation on the LPC55S69 slave, a reset is required. The slave also be reset after probing available I2C devices.
The experimental hardware connection is shown in the figure.
Hope this helps you.
BR
Xu Zhang