Reg: LPC845 ADC maximum Negative Voltage to withstand.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reg: LPC845 ADC maximum Negative Voltage to withstand.

1,103 次查看
PK_1114
Contributor II

Hai,

What is the maximum allowable negative voltage on the ADC Pin in LPC845 Micro controller operating on the +3.3V.

Thank You,

B Pavan Kumar  

标记 (1)
0 项奖励
回复
2 回复数

1,043 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi PK_1114 

According to datasheet, ADC anolog input limit is as below

ZhangJennie_0-1698221653986.png

It is recommended to connect an overvoltage protection diode between the analog input pin and the voltage supply pin.

Have a nice day,

Jun Zhang

0 项奖励
回复

1,074 次查看
PK_1114
Contributor II
Hi,

Is there any Reverse Protection in the LPC845 ADC pin, if there what is it voltage tolerance. I need to give the Sinusoidal wave to the ADC.

Thank You,
B Pavan Kumar
0 项奖励
回复