Reading LPC17xx flash memory via ISP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reading LPC17xx flash memory via ISP

1,037 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ezharkov on Tue Jun 10 16:10:30 MST 2014
I'm trying to read LPC1765 flash memory via ISP IAP. Getting the correct data for everything except the first 512-bytes block. I.e., "R 512 512" works fine. But "R 0 512" returns garbage (correct reply checksum, but not the data that I expect). The same program works fine with LPC1788.
标签 (1)
0 项奖励
回复
1 回复

966 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ezharkov on Wed Jun 11 06:39:44 MST 2014
OK, this must have something to do with the boot ROM mapping. Still not clear why this works on LPC1788.
0 项奖励
回复