RTC calibration in LPC55S69

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTC calibration in LPC55S69

跳至解决方案
1,208 次查看
gnichimohamed
Contributor III

Hello,

In the LPC55S69 there is no mentioning of RTC calibration, do you have any idea how we can do it?

Thanks for the help!

0 项奖励
回复
1 解答
1,200 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,201 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello gnichimohamed,

 

Sorry LPC55s69 doesn't support RTC calibration. 

32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power
domain. A timer in the RTC can be used for wake-up from all low power modes
including deep power-down, with 1 ms resolution. The RTC is clocked by the
32 kHz FRO or 32.768 kHz external crystal.

 

BR

Alice

0 项奖励
回复