RTC Operation in power down mode in LPC546xx Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC Operation in power down mode in LPC546xx Microcontroller

Jump to solution
840 Views
prasannanaik
Contributor III

Hi,

   I have a query regarding operation of RTC in LPC546. I want to know whether the RTC counter register (COUNT) will keep on updating or not in device power down mode (i.e no VDD only VBAT). The datasheet mentions that the . RTC module and the oscillator that drives it, runs directly from the device power pins. Does this means that the RTC counter won't be updated in device power down mode(i.e when only Vbat is present).

I have attached the sceenshot of the datasheet for reference.

Thanks and best regards,

Prasanna

Labels (1)
0 Kudos
1 Solution
753 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prasanna,

You are right, the RTC counter register (COUNT) will keep on updating in device power down mode (i.e no VDD only VBAT).

BR

XiangJun Rong

View solution in original post

0 Kudos
2 Replies
754 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prasanna,

You are right, the RTC counter register (COUNT) will keep on updating in device power down mode (i.e no VDD only VBAT).

BR

XiangJun Rong

0 Kudos
753 Views
prasannanaik
Contributor III

Hi xiangjun.rong‌,

   Thanks for your help.

    I verified the same on LPC546xx development board OM30192.

Thanks and best regards,

Prasanna

0 Kudos