RC663-LPC1227-Polling - built's ok but the LPCXpresso gives me the following error :river v8.2 (Sep 5 2016 10:12:38 - c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RC663-LPC1227-Polling - built's ok but the LPCXpresso gives me the following error :river v8.2 (Sep 5 2016 10:12:38 - c

830 Views
bd2000
Contributor I

Hi I need help to solve problems with my ide unable to program flash and the following error comes up:- Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink.exe build 725) Pc: ( 0) Reading remote configuration Pc: ( 5) Remote configuration complete Wc: ============= SCRIPT: LPC12XXConnect.scp ============= Wc: LPC12XX Connect Script Wc: DpID = 2BA01477 Wc: APID = 0x24770011 Wc: ============= END SCRIPT ============================= Xe: Nc: Probe Firmware: LPC-Link Probe v1.3 (NXP - LPC-Link) Nc: Serial Number: HID64HS12 Nc: VID:PID: 1FC9:0007 Nc: USB Path: Pc: ( 30) Emulator Connected Xc: Pc: ( 40) Debug Halt Pc: ( 50) CPU ID Nc: Emu(0): Connected&Reset. DpID: 2BA01477. CpuID: 410FC230. Info: <None> Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled. Nc: inspected v.2 On-chip Flash Memory C:\nxp\LPCXpresso_8.2.2_650\lpcxpresso\bin\Flash\LPC11_12_13_128K_8K.cfx Nc: image 'LPC11_12_13 (128K Flash, min 8K RAM) Jun 21 2016 11:53:37' Nc: NXP: LPC1227/301 Part ID: 0x00000000 Pc: ( 65) Chip Setup Complete 'ipconfig.exe' is not recognized as an internal or external command, operable program or batch file. 'cscript.exe' is not recognized as an internal or external command, operable program or batch file. Nt: Connected: was_reset=false. was_stopped=true Cr:f LPCXpresso Free License - Download limit is 8K (UNREGISTERED) Pc: ( 70) License Check Complete Et:53: License does not permit flash operations from command line Pc: (100) Target Connection Failed

0 Kudos
3 Replies

731 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Deepak ,

I am following this case.

Also, you should be able to see my recommendations on the tickect.

Regards,

Diego.

0 Kudos

731 Views
bd2000
Contributor I

Thanks Con Verse.

In the LPCxpresso ide when i try to create serial number and activate, the bower open and sends a request for the key, but then it hangs and does not do any think in the browser.

I have a 32 bit - windows 7 and the MCUXpresso only supports 64 bit machine. Also the RC663-LPC1227-Polling demo in the application mentions that any newer version will not work with the demo. i.e in section this is what is said:-

For development please use the LPCXpresso version 4.x. Newer versions of the IDE are known not to work correctly with the provided software examples.

I have looked on the internet and raised a support ticket to NXP, but no Joy! see attached guide.

Does any one know how to activate a key for version 4 LPCXpresso? or will MCUXpresso run the demo software.

Many thanks in advance for your support.

0 Kudos

731 Views
converse
Senior Contributor V

You've not activated your LPCXpresso, which is why you get this error. See

https://community.nxp.com/thread/388959 

But, you should now use MCUXpresso as this has replaced LPCXpresso and you do not need to register it.

0 Kudos