Programming spec of LPC11U35FBD48 and LPC11U36FBD48

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming spec of LPC11U35FBD48 and LPC11U36FBD48

1,634件の閲覧回数
Leap_Electronic
Contributor II

Dear NXP team,

 

This is Austin for Leap Electronic.

Our customer All Point in Brazil need to add  LPC11U35FBD48 and LPC11U36FBD48 into our automated Programming System.

Please provide both of  LPC11U35FBD48 and LPC11U36FBD48 programming specification. 

The spec must has the following  information

1. The connecting diagram and instruction for the programming, included I/O pin, POWER pin, CLK pin.

2. AC/DC electrical specifications and timing for programming.

3. How to enter the programming mode process and the timing.

4. The flow and the timing for the function of Erase, Program, Read, and Protect.

5. The memory map, Option and Config for the programming.

6. The simple program for the programming.

Thanks in advance,

 

Best regards,

Austin

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,594件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the LPC11U35/36 do not have EVK board.

I suppose that you can refer to the schematics of LPC11U68-EVK, which I attach it here.

You have to pay attention to the following items as a minimum system.

1)power supply pins

2)SWD connector

3)crystal design

4)ISP pins

The LPC11u35/36 has ROM code, which includes the api function to erase/program flash.

Do you want to erase/program flash with SWD port or in ISP mode, in ISP mode, you can use uart or USB port to program/erase.

BR

XiangJun Rong

0 件の賞賛
返信