Problems with LPCOpen 2.10 on LPC1788/LPC4078 and LwIP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with LPCOpen 2.10 on LPC1788/LPC4078 and LwIP

2,525件の閲覧回数
carlobramini
Contributor II

Hello,

I tried to make working LPCOpen 2.10 with some boards based on LPC1788 and LPC4078, but I got many troubles with networking and LwIP.

Actually, the first malfunction was the inability to detect link status.

After long debugging, I have identified some suspicious code, so I would be pleasured to know your opinion.

Inside  lpc_chip_177x_8x\src\enet_17xx_40xx.c there is this declaration:

/* Divider index values for the MII PHY clock */
STATIC const uint8_t EnetClkDiv[] = {4, 6, 8, 10, 14, 20, 28, 36, 40, 44,
                                     48, 52, 56, 60, 64};‍‍‍‍‍‍

However, the register MAC_MCFG is described inside UM10470 in this way:

Clock Select Bit 5 Bit 4 Bit 3 Bit 2 Maximum AHB clock supported
Host Clock divided by 4 0 0 0 x 10
Host Clock divided by 6 0 0 1 0 15
Host Clock divided by 8 0 0 1 1 20
Host Clock divided by 10 0 1 0 0 25
Host Clock divided by 14 0 1 0 1 35
Host Clock divided by 20 0 1 1 0 50
Host Clock divided by 28 0 1 1 1 70
Host Clock divided by 36 1 0 0 0 80 [1]
Host Clock divided by 40 1 0 0 1 90 [1]
Host Clock divided by 44 1 0 1 0 100 [1]
Host Clock divided by 48 1 0 1 1 120 [1]
Host Clock divided by 52 1 1 0 0 130 [1]
Host Clock divided by 56 1 1 0 1 140 [1]
Host Clock divided by 60 1 1 1 0 150 [1]
Host Clock divided by 64 1 1 1 1 160 [1]

So, the table seems wrong because 00000 and 00001 both divided by 4, and this shifted everything by one position.

After correcting the code to:

/

* Divider index values for the MII PHY clock */
STATIC const uint8_t EnetClkDiv[] = {4, 4, 6, 8, 10, 14, 20, 28, 36, 40, 44,
                                     48, 52, 56, 60, 64};‍‍‍‍‍‍

I finally got correct frequency from MDC pin.

Next, it happened that the driver was unable to read from MDIO pin.

The writes happened successfully, but the reads didn't.

I discovered that because the samples were unable to detect when the cable was extracted or inserted.

After many hours of tries, I think that I discovered how to make it working.

From the UM10470, the P1[16 to 17] are assigned to a "Type W IOCON register" and actually it clearly states that bit 7 must be set to 1 for normal operation.

Inside lpc_board_ea_devkit_1788\src\board_sysinit.c, there is this code:

    {0x1, 16, (IOCON_FUNC1 | IOCON_MODE_INACT)},
    {0x1, 17, (IOCON_FUNC1 | IOCON_MODE_INACT)},
‍‍‍‍‍‍

But this is wrong because it does not set bit 7 to 1.

After changing to:

    {0x1, 16, (IOCON_FUNC1 | IOCON_MODE_INACT | 0x80)},
    {0x1, 17, (IOCON_FUNC1 | IOCON_MODE_INACT | 0x80)},
‍‍‍‍‍‍

the access to the registers has been fixed.

What do you think about these changes?

At the corrent state, the samples using LwIP with raw API work fine.

Sadly, the samples using LwIP and FreeRTOS still do not work.

I really hope that somebody could give some advices for making working the LwIP samples with FreeRTOS, because at the moment and many hours of debugging I'm a bit out of idea.

Thank you very much for your time.

Sincerely.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

2,333件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Carlo,

 

Thanks for reporting this issues. I would like to test this myself, please wait a little while I do some work on my side.

 

Best regards,

Felipe

0 件の賞賛
返信

2,333件の閲覧回数
carlobramini
Contributor II

Hello,

I was wondering if there are some news about this topic.

Thank you very much for your time.

 

Sincerely.

0 件の賞賛
返信

2,333件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Carlo,

 

Sorry for my delayed response. Please check my comments below.

 

I have LPC4088 QuickStart Board on my side and I used the LPCOpen library from the following link.

 

https://www.embeddedartists.com/wp-content/uploads/2018/06/lpcopen_2_10_lpcxpresso_arm_university_40...

 

Regarding your first workaround, I tested this without modification and the example was running fine, the link status was always detected but this will depend on the clockRate you set in Chip_ENET_SetupMII.

 

Your second workaround is correct, actually the following is already implemented in lpc_board_ea_devkit_4088 library that I used. It is the same solution that you did on your side.

 

{0x1, 16, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)},
{0x1, 17, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)},‍‍

 

Lastly, I checked and tested on my side the lwip_tcpecho_freertos example and I did not see any issue on my side. Maybe you can give more details regarding the errors you are seeing.

 

I hope this helps.

 

Best regards,

Felipe

0 件の賞賛
返信