Problem with LPC4330-Xplorer and LPC-Link(HID)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with LPC4330-Xplorer and LPC-Link(HID)

465 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Willi.L on Fri Jun 28 05:59:45 MST 2013

I have a follow problem:


I use LPCExpresso (v5.2.4) and LPCXplorer4330.


If I debug the LPC4330-Xplorer_LedToggle-Example (without changes) with LPC-Link2 (Debugger set to RedProbe), it works fine.


If I debug the same axf.-file with LPC-Link (Debugger set to LPC-Link(HID)), it works not correct. I can debug, but the processor stays in systick_delay(),


because the SysTick_Handler(void) will not be run.


Have anyone idee, what is the cause?

标签 (1)
0 项奖励
回复
0 回复数