Problem in waking up from deep sleep in LPC4330

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in waking up from deep sleep in LPC4330

1,225 次查看
cescvaro
Contributor II

Hi all,

 

I'm working with a custom board with an LPC4330 (flashless) with a SPIFI flash.

My problem happens when the micro wake up: the wake up signal came from the WAKEUP0 pin, the micro detect it and as soon as it wakes up, I restore the clocks as in chapter 13.1.1.2 Changing the BASE_M4_CLK after waking up from deep-sleep or power-down modes of the Datasheet.

 

The procedure gave me no problem, the micro doesn't get stuck in any of the operation (previously I had problems during startup due to not long enough wait cycles between some operation) but the very next function call after setting up the clocks results in losing debug connection (PC = 0xDEADBEEF or something similar).

This is the function before going in deep sleep:

 

/**
 * Set IRC as source clock fo all the output clocks & power down
 * before going to 'Deep Sleep'/'Power Down'/'Deep Power Down' modes
 */
void SystemSetupClocking_SleepPowerDown(void)
{
    int i;
    /* Shutdown perpheral clocks with wake up enabled */
    Chip_Clock_StartPowerDown();

    /* Get state of individual base clocks & store them for restoring.
     * Sets up the IRC as base clock source
     */
    for (i = 0; i < (sizeof(InitClkStates) / sizeof(InitClkStates[0])); i++)
    {
        /* Get the Base clock settings */
        Chip_Clock_GetBaseClockOpts(InitClkStates[i].clk, &InitClkStates[i].clkin,
                                    &InitClkStates[i].autoblock_enab, &InitClkStates[i].powerdn);

        /* Set IRC as clock input for all the base clocks */
        Chip_Clock_SetBaseClock(InitClkStates[i].clk, CLKIN_IRC, InitClkStates[i].autoblock_enab,
                                InitClkStates[i].powerdn);  /* wow that's hardcore */
    }

    /* Set IRC as clock source for SPIFI */
    Chip_Clock_SetBaseClock(CLK_BASE_SPIFI, CLKIN_IRC, true, false);

    /* Set IRC as source clock for Core */
    Chip_Clock_SetBaseClock(CLK_BASE_MX, CLKIN_IRC, true, false);

    /* Power down the main PLL */
    Chip_Clock_DisableMainPLL();
    Chip_Clock_DisablePLL(CGU_USB_PLL);
    Chip_Clock_DisableCrystal();
}

 

And this is the function to restore pll and clocks:

    uint16_t i;

    PLL_PARAM_T ppll;

    Chip_Clock_GetMainPll(&ppll);

    /* 1 Enable the crystal oscillator */
    Chip_Clock_EnableCrystal();
    Chip_Clock_EnableMainPLL();

    /* 2 Select the crystal as clock source for BASE_M4_CLK */
    ppll.srcin      = CLKIN_CRYSTAL;
    /* 3 set autoblock bit */
    ppll.autoblock  = 1;            /* */

    /* 4a Reconfigure pll: M and N */
    Chip_Clock_CalcMainPLLValue(Desired_Freq, &ppll);  /* calc of param for pll for desired freq - results in ppll !!!! */

    /* 4b: crystal as clock source for PLL1 */
    //ppll.srcin      = CLKIN_CRYSTAL;
    Chip_Clock_SetupMainPLL(&ppll); // yeah set again
    Sysinit_delay(1000);               /* mine */

    /* 5 wait pll lock */
    while(!Chip_Clock_MainPLLLocked()) {}

    /* 6 set direct = 0 psel = 0*/
    ppll.ctrl &= ~(1<<7);   /* clears DIRECT */
    ppll.psel = 0;          /* psel to 0 */


    /* 7 select pll1 as base_m4_clk source */
    Chip_Clock_SetBaseClock(CLK_BASE_MX, CLKIN_MAINPLL, true, false);   /* passing 3rd as true = AUTOBLOCK = true */

    /* 8 wait 50 us */
    Sysinit_delay(0x4000); /* 4800*/

    /* 9 set direct to 1 */
    ppll.ctrl |= (1 << 7);   /* set DIRECT */
    ppll.psel = 0;
    Chip_Clock_SetupMainPLL(&ppll); /* Set DIRECT to operate at full frequency */

    Sysinit_delay(0x4000); /* 4800*/
    while(!Chip_Clock_MainPLLLocked()) {}

    Chip_Clock_SetBaseClock(CLK_BASE_SPIFI, CLKIN_IDIVE, true, false);

    for (i = 0; i < (sizeof(InitClkStates) / sizeof(InitClkStates[0])); i++)
    {
        Chip_Clock_SetBaseClock(InitClkStates[i].clk, InitClkStates[i].clkin,
                                InitClkStates[i].autoblock_enab, InitClkStates[i].powerdn);
        //Chip_sysinit_delay(1000);   /* mine */
    }

 

Any suggestion?

 

If I reset the micro, it clearly works fine.

标签 (1)
0 项奖励
回复
3 回复数

1,209 次查看
cescvaro
Contributor II

Hi Alice,

 

thank you for the answer.

I'm not debugging during deep sleep, I try to connect to the micro after the wake up signal and debugger shows me PC 0xDEADBEEE, that it usually happens when something bad occured (I think related to memory access or pll not well configured).

I've also put a debug cycle to be able to perform the operation step by step after waking up

    volatile bool wait_for_debug = false;

    while(!wait_for_debug)
    {
        __NOP();
    }

 

And then, by debugging, pll settting looks fine and is executed without the micro getting stuck, but the system lose the connection debug (I guess the micro goes into an indefinite state - HardFault is not hit!) when I'm calling this function

Chip_EVRT_DeInit();

(I'm using this version of lpcopen for 43xxx: Thu 05/15/2014 ).

If I remove this call, the system doesn't get lost, but I'm still investigating because looks like some IRQ are not working properly - checking if I'm not re enabling it or what.

 

This call just write some 0xFF in a register

 

/**
 * @brief	De-initializes the EVRT peripheral
 * @return	Nothing
 */
STATIC INLINE void Chip_EVRT_DeInit(void)
{
	LPC_EVRT->CLR_EN    = 0xFFFF;
	LPC_EVRT->CLR_STAT  = 0xFFFF;
}

Why it cause the sytem to get lost ? Any specification about wait time/cycle after a wake up from deep sleep?

 

Reading this https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-hard-fault-after-reset-from-application/m-... there could be "issue" about the voltage of internal regulators.

 

BR,

fv

0 项奖励
回复

1,200 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello fv,

Please share your whole project and the steps that how to reproduce your issue.

 

BR

Alice

0 项奖励
回复

1,215 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cescvaro,

From User Manual UM10503-> P1377:

• Due to limitations of the Cortex-M4 integration, the LPC43xx cannot wake up in the
usual manner from Deep Sleep and Power-down modes. Do not use these modes
during debug.

 

BR

Alice

0 项奖励
回复