Presentation material on the LPC80x Switch Matrix

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Presentation material on the LPC80x Switch Matrix

Jump to solution
1,425 Views
drsmith_yorku
Contributor III

Hi,

I'm looking for the PPTX slides for the presentation on the LPC80x Switch Matrix that are featured in the video on the NXP webpage (LPC80x微控制器系&#210|NXP ).  Some of the images are really hard to view because they are in low resolution.

thanks!

James

Labels (2)
0 Kudos
Reply
1 Solution
1,301 Views
soledad
NXP Employee
NXP Employee

Please check the attachment. 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,301 Views
drsmith_yorku
Contributor III

Thanks!  That's perfect.

all the best,

James

0 Kudos
Reply
1,302 Views
soledad
NXP Employee
NXP Employee

Please check the attachment. 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply