Port and pin information on LCD Reset (Port2, Pin27) on the document?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port and pin information on LCD Reset (Port2, Pin27) on the document?

2,816 Views
yasokada
Contributor II

My Environment:

- OS: Ubuntu 18.04 LTS

- Board: LPCXpresso54628

- IDE: MCUXpresso IDE v11.0.1 [Build 2563] [2019-09-01]

I examined touch_cursor.c from SDK example.

I found the following .

```

    /* Trigger LCD reset */
    GPIO_PinInit(GPIO, 2, 27, &pin_config);
    GPIO_PinWrite(GPIO, 2, 27, 1);

```

I searched information about the Port2, Pin 27 on documents, but failed to find.

I have read the docuemnts:

A. LPC546XX.pdf

B. RK043FN02H-CT.pdf

C. UM10912.pdf

D. UM11035.pdf

Where can I find the information about LCD reset port and pin on which documents?

Thanks in advance.

Labels (1)
7 Replies

2,637 Views
yasokada
Contributor II

Dear XiangJun rong

Thank you again for your reply.

But that's now what I was looking for.

Connecting information (the pin information on the the Cap Touch RK043FN02H-CT LCD display, connected to the Port 2-27 of LPCXpresso54628) may be the information.

I spent too much  time only for seeking information on this without success, looking the documents and forum Q and As.

I found that J16 and J17 on LPCXpresso54628 are related to the LCD display, but the old forum question on the J16 is unanswered.

(the UM11035.pdf do not have the figure on the J16 and J17, maybe, only texts J16 and J17)

I gave up on this investigation.

Anyway, thank you for your countless help.

PS.

I have experienced MSP430, STM32 (a little) and other MCUs. I understand the GPIO initilization and high and low state change for the reset.

The connecting information is missing.

0 Kudos
Reply

2,637 Views
yasokada
Contributor II

Here is the question unanswered, about the J16 and J17.

The board is different but the LCD connection maybe similar?

https://community.nxp.com/thread/514219 

0 Kudos
Reply

2,637 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yas,

As you know that the LPCXpresso54628 board can interface with LCD and Cap Touch panel, in other words, the LCD module provides two interface connector, one is LCD connector J16, another is cap touch interface connector J17. The LCD can display picture/text with J16, you can touch the LCD film on the LCD screen, the touch inf can be transferred to LPC processor via I2C interface via J17, so you can scroll, rotate on the cap touch screen film.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

2,637 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yas,

Pls refer to the UM10912.pdf and check the Chapter 10: LPC546xx I/O pin configuration (IOCON), which describes the pin assignment.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply

2,637 Views
yasokada
Contributor II

Dear XiangJun 

Thank you for your reply.

I have read that part. But, it's not clear how the [LCD_VD[9] (PIO2_27) works as a reset.

The connecting diagram or table between the LPCXPresso54628 and the Rocktech LCD module may help,

but I didn't find it on the documents, not on the Datasheet for Rocktech LCD module REV1.0 also.

The sentence on the SDK example looks like a magic. I do not want to use it without knowing the detail as an engineer.

0 Kudos
Reply

2,637 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yas,

Pls refer to the following section, during and after Reset, the IOCON register  for all PIO2 port pins is 0x0320, which means that the PIO2 pins are in GPIO mode, the default value of GPIO port direction register is 0, so the PIO2 pins are in GPIO and input mode during/after Reset.

Hope it can help you

BR

Xiangjun Rong

pastedImage_1.png

2,637 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, yas,

I am sorry, I misunderstood your original question previously, as you know that the PIO2_27 pin is connected to the Reset pin of Cap Touch RK043FN02H-CT LCD display.

As you know that PIO2_27 can be configured as GPIO pin, after reset, the application code is run, in the application code, if you need to display something and touch the screen, you can configure PIO2_27 pin  as GPIO and output mode with the line:

GPIO_PinInit(GPIO, 2, 27, &pin_config);

then you can clear the PIO2_27 to reset the Cap Touch RK043FN02H-CT LCD display with the line:

GPIO_PinWrite(GPIO, 2, 27, 0);

//because of an external pull-down resistor and the pin is in input mode during/after chip Reset, so the PIO2_27 will //be in LOW logic, so the line maybe removed.

//after a programmable delay like

delay();

//then set the PIO2_27 pin with the line:

GPIO_PinWrite(GPIO, 2, 27, 1);

//It is okay.

During and after processor Reset, the PIO2_27 is in input mode, because of a pull-down resistor, the pin is LOW. after the above application code is run, the PIO2_27 will finish LOW logic, Delay, High logic, the Cap Touch RK043FN02H-CT LCD display. will be Reset.

Hope it can help you

BR

XiangJun rong