Please help me with LCD(16*2) driver code and please guide me in detail(I am beginer for uclinux device drivers)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Please help me with LCD(16*2) driver code and please guide me in detail(I am beginer for uclinux device drivers)

465 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by amar on Thu Mar 21 22:12:58 MST 2013
Hi,

I have LPC1788 EVB board with uclinux running on in it.


now i want to drive an LCD(16*2) with lcd driver code.?

I am new for device drivers plaese help me what are the changes need to do in file system to add my lcd driver..?

my LCD connections are:

data pins are connected to P0.27 to P0.31 and enable pin of LCD is connected to LPC port P2.4
RS to P2.1 and w/r is grounded.

Please help me with driver code and please guide me in detail(I am beginer for device drivers with uclinux)
标签 (1)
0 项奖励
回复
0 回复数