Hi,
programming custom board with LPC11U68JBD100.
I initialize PININT on port 0 pins 2 and 20, port 2 pins 2 and 5 using these functions:
Chip_GPIO_Init(LPC_GPIO);
Chip_GPIO_SetPinDIRInput(LPC_GPIO, ...
Chip_Clock_SetIOCONFiltClockDiv(0, 64);
Chip_IOCON_PinMuxSet(LPC_IOCON, ... (IOCON_FUNC0 | IOCON_MODE_PULLUP | IOCON_CLKDIV(0) | IOCON_HYS_EN | IOCON_S_MODE(3))
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_PINT);
Chip_SYSCTL_SetPinInterrupt(n, ...
Chip_PININT_ClearIntStatus(LPC_PININT, PININTCH(n));
(n is 0 to 3)
NVIC_ClearPendingIRQ(name);
NVIC_EnableIRQ(name);
(names are PIN_INT0_IRQn to PIN_INT3_IRQn)
Created four handlers ( PIN_INT0_IRQHandler() ... PIN_INT3_IRQHandler() )
Handlers execute:
Chip_PININT_ClearIntStatus(LPC_PININT, PININTCH(int number));
and blink with LEDs.
int 0 and 1 (port 0.2 and 0.20) working properly, LEDs blinks after pin pulled low
int 2 and 3 (port 2.2 and 2.5) not working
What's wrong?
Thanks
已解决! 转到解答。
Solved:
My code is OK.
Wrong is function Chip_SYSCTL_SetPinInterrupt
from examples archive lpcopen_2_06_lpcxpresso_nxp_lpcxpresso_11u68.zip
distributed with LPCXpresso v8.1.4_606
lpc_chip_11u6x\src\syscon_11u6x.c
Wrong, original version, working only with port 0:
void Chip_SYSCTL_SetPinInterrupt(uint32_t intno, uint8_t port, uint8_t pin){
if (port == 0) {
/* Pins P0.1 to P0.23 only */
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) pin;
} else {
/* P1.1 to P1.31 and P2.0 to P2.7 */
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) ((port - 1) * 32 + pin);
}
}
Repaired:
void Chip_SYSCTL_SetPinInterrupt(uint32_t intno, uint8_t port, uint8_t pin){
if (port == 0) {
// Pins P0.0 to P0.23 only
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) pin;
} else if (port == 1) {
// P1.0 to P1.31
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) (24 + pin);
} else {
// P2.0 to P2.7
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) (24+32 + pin);
}
}
Solved:
My code is OK.
Wrong is function Chip_SYSCTL_SetPinInterrupt
from examples archive lpcopen_2_06_lpcxpresso_nxp_lpcxpresso_11u68.zip
distributed with LPCXpresso v8.1.4_606
lpc_chip_11u6x\src\syscon_11u6x.c
Wrong, original version, working only with port 0:
void Chip_SYSCTL_SetPinInterrupt(uint32_t intno, uint8_t port, uint8_t pin){
if (port == 0) {
/* Pins P0.1 to P0.23 only */
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) pin;
} else {
/* P1.1 to P1.31 and P2.0 to P2.7 */
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) ((port - 1) * 32 + pin);
}
}
Repaired:
void Chip_SYSCTL_SetPinInterrupt(uint32_t intno, uint8_t port, uint8_t pin){
if (port == 0) {
// Pins P0.0 to P0.23 only
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) pin;
} else if (port == 1) {
// P1.0 to P1.31
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) (24 + pin);
} else {
// P2.0 to P2.7
LPC_SYSCTL->PINTSEL[intno] = (uint32_t) (24+32 + pin);
}
}