OpenOCD support for LPC55S69 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenOCD support for LPC55S69 EVK

2,951 次查看
cgarcia
Contributor II

Is there OpenOCD support for LPC55S69 EVK board ? based on CMSIS-DAP probe

标签 (1)
0 项奖励
回复
5 回复数

2,942 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

This is belongs to 3rd party. We never declaim we support OpenOCD.  I suggest you using the MCUXpresso IDE associating with the JLINK or CMSIS DAP interface to download the code.


OpenOCD can support many company MCUs, The supported chips are listed there.

http://openocd.org/

 

BR

Alice

0 项奖励
回复

2,933 次查看
cgarcia
Contributor II

Hi Alice,

Thanks for replaying, yes MCUXpresso IDE is a good option however I am working in a project that support multiple vendors and a generic open tool is a good option to keep common environment.

I think just I have to find a proper LPC55S69 config file for openocd, if you know someone from community has worked about it, please let me know.

Thanks  

0 项奖励
回复

1,660 次查看
Aisha
Contributor I

Hey , 

I am working on the same project as you were , can you tell me how much did you progress ahead and the basic procedure with which you accessed LPC55sx family using openocd?

0 项奖励
回复

2,929 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

I searched the community , also talking internal with my other  colleague, we haven't meet customer use this as so far, sorry for the inconvenient .

 

BR

Alice

0 项奖励
回复

2,925 次查看
cgarcia
Contributor II

Alice,

I haven't found something about it neither, thanks I appreciate your help.

Thank you.

0 项奖励
回复