OTA support on LPC55S69JBD100E interfacing with WM02C(nRF7002)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTA support on LPC55S69JBD100E interfacing with WM02C(nRF7002)

353件の閲覧回数
Laks489
Contributor I

Hi

Does the NXP-LPC55S69JBD100 support OTA updates through bootloader when connected to the WM02C (nRF7002) via SPI? Please explain the OTA update process.

ラベル(1)
0 件の賞賛
返信
1 返信

340件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hi @Laks489,
Yes, the LPC55S69 supports OTA, I highly recommend the chapter 6 and 7 of these users guide where the OTA is better explicated. 

Also, the SDK (version 24.12) provides an example called "mcuboot_opensource" where could be helpful.
BR
Habib

0 件の賞賛
返信