OTA support on LPC55S69JBD100E interfacing with WM02C(nRF7002)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA support on LPC55S69JBD100E interfacing with WM02C(nRF7002)

459 Views
Laks489
Contributor I

Hi

Does the NXP-LPC55S69JBD100 support OTA updates through bootloader when connected to the WM02C (nRF7002) via SPI? Please explain the OTA update process.

Labels (1)
0 Kudos
Reply
1 Reply

446 Views
Habib_MS
NXP Employee
NXP Employee

Hi @Laks489,
Yes, the LPC55S69 supports OTA, I highly recommend the chapter 6 and 7 of these users guide where the OTA is better explicated. 

Also, the SDK (version 24.12) provides an example called "mcuboot_opensource" where could be helpful.
BR
Habib

0 Kudos
Reply