OM13054: Failed on connect: Ee(36). Could not connect to core

cancel
Showing results for 
Search instead for 
Did you mean: 

OM13054: Failed on connect: Ee(36). Could not connect to core

104 Views
ferentes
Contributor I

Hello,

I am trying to debug sample applications on a OM13054 board with LPCXpresso IDE.

Getting a message: Failed on connect: Ee(36). Could not connect to core.

The red LED on the board is slowly flashing.

What could be the reason? Is the board MCU defective? 

Labels (1)
0 Kudos
1 Reply

38 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ilia malamoud,

How do you debug the board of  OM13054 ?

Please pay attention, there is no on debugger on board,  we need use external debugger to debug it.

And the LPCxpresso IDE only support LPClink( CMSIS-DAP ) debug.

Recommend using MCUXpresso IDE , it support P&E, Jlink and CMSIS-DAP.

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP     


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos