Hello,
I am trying to debug sample applications on a OM13054 board with LPCXpresso IDE.
Getting a message: Failed on connect: Ee(36). Could not connect to core.
The red LED on the board is slowly flashing.
What could be the reason? Is the board MCU defective?
Hello ilia malamoud,
How do you debug the board of OM13054 ?
Please pay attention, there is no on debugger on board, we need use external debugger to debug it.
And the LPCxpresso IDE only support LPClink( CMSIS-DAP ) debug.
Recommend using MCUXpresso IDE , it support P&E, Jlink and CMSIS-DAP.
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------