Not able to copy more than 8 kB data at a time into Flash bank LPC1833

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to copy more than 8 kB data at a time into Flash bank LPC1833

ソリューションへジャンプ
905件の閲覧回数
ketulpatel
Contributor II

Hello,

We are using LPC1833 in our project. In which we are flashing an image of 87 kB size.

But not able to use more than 8 kB of Flash Buffer size to flash the image.

How we can use more than 8 kB of buffer for the same?

Thanks,
Ketul

タグ(1)
0 件の賞賛
返信
1 解決策
850件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

2 返答(返信)
822件の閲覧回数
ketulpatel
Contributor II

Thank You!

0 件の賞賛
返信
851件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the supported values of bytes to be written are the ones listed in the reference manual.

Omar_Anguiano_0-1627685148179.png


I apologize for the inconvenience this may cause you, if you have more questions do not hesitate to ask me.
Best regards,
Omar