Net-snmp 5.4.3 error at the time of installation for porting into linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Net-snmp 5.4.3 error at the time of installation for porting into linux

1,431 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MOHAMMAD BIYABANI on Thu Mar 21 21:50:26 MST 2013
Hi,
I am Trying to install NET-SNMP 5.4.3 but getting the errors.The problem is when i was installed NET-SNMP then it is showing

../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_null_context'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_null'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_get_bulk_to_next_handler'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_old_api'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_init_helpers'
collect2: ld returned 1 exit status
make[1]: *** [snmptrapd] Error 1
make[1]: Leaving directory `/home/mohan/net-snmp-5.4.3/apps'
make: *** [subdirs] Error 1

Initially it was also shown the
/usr/bin/ld: cannot find -lperl error
But that was rectified by installing libperl-dev package. I have tried to rectify remaining two errors but the problem has not solved.
I attached the snap shot of error message also it is useful to give answer.

Thanks & Regards,

MOHAMMAD BIYABANI.
标签 (1)
0 项奖励
回复
0 回复数