Need the library file for lpc2148 for LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need the library file for lpc2148 for LPCXpresso IDE

1,395件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Asim27902 on Sun Dec 28 00:27:28 MST 2014
Hello All,

I'm currently using the free edition of LPCXpresso, I have observed that LPC2148 is not supported with LPCXpresso, since my program size for LPC2148 is smaller than 128KB, I wanted to use LPCXpresso for development with LPC2148. ( It would look something like this ex. CMSISv2p00_LPC2xxx) If any of you can provide me with the file, I would be thankful.
regards,
Asim Sayed
Assistant Professor
AISSMSCOE, Pune
Maharashtra, India
ラベル(1)
0 件の賞賛
返信
1 返信

1,086件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Dec 28 01:25:55 MST 2014
There is no such file.

CMSIS stands for Cortex Microcontroller ... And LPC2000 is not Cortex.

You will find some header files in a zip file called old headers I. The examples directory. But there is no library.
0 件の賞賛
返信