Need of working SPI driver for LPC11A04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need of working SPI driver for LPC11A04

1,212件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RatheeshT on Tue Jan 05 03:27:58 MST 2016
Hi, 

    I tried SPI driver in loop back mode , it is working fine. To communicate with external device, i tried to use SPI in polling and interrupt modes. I cannot find it is working or not.
Please tell me how can i  check ?

Specification -;

SPI frequency - 8MHZ (set by me )
IDE used - LPCXpresso v7.9 2_493  
Platform - windows 7

Thanks in advance

Regards,

Ratheesh T
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RatheeshT on Tue Jan 05 23:19:54 MST 2016
HI,

First thank you for quick response, i will try on board to board communication.

I am testing SPI with older version v1.03. Is it available SPI V2.03 ( latest version ). Pls give me the exact link for latest version of SPI driver.


Thanks & regards ,
Ratheesh T
0 件の賞賛
返信

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Jan 05 08:56:34 MST 2016
Hi Ratheesh T,
If you have two board you can make LPC on one board as a master and the LPC on another board as a slave. If you do not have two board you can communicate with any SPI-based EEPROM.
0 件の賞賛
返信