Need calrification about the voltage tolerence of LPC1788 GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need calrification about the voltage tolerence of LPC1788 GPIO

905件の閲覧回数
mano_hw
Contributor I
Hi

For general purpose digital input/output pins the input voltage tolerance is 5v only if VDD>=2.4v 

if VDD<2.4v then the input voltage tolerance is 3.6v.

What is the 2.4V means. Is that the controller input voltage or the reference voltage?

I have a ultrasonic sensor which will work on the input voltage of 5V. We have two pins(Trigger and Echo) . In these 2 pins the output voltage will be only 5V. Whether i can interface these pins with controller? Will it work?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

834件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check my replay here Need calrification about the voltage tolerence of LPC1788 GPIO 


Have a great day,
Sol>
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信