Need calrification about the voltage tolerence of LPC1788 GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need calrification about the voltage tolerence of LPC1788 GPIO

1,973 次查看
mano_hw
Contributor I

Dear Friends

We need some clarification about LPC1788 GPIO PIN input Voltage tolerance  ?

we already referred the data sheet that indicates the input voltage tolerance is 5v.

in Limiting values tables

5 V tolerant digital
V
DD(3V3)
2.4V
So please confirm I can give 5V input to the LPC1788 GPIO ?
Thanks and regards
Mano
标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

1,776 次查看
mano_hw
Contributor I

Hi

What is the 2.4V means. Is that the controller input voltage or the reference voltage?

I have a ultrasonic sensor which will work on the input voltage of 5V. We have two pins(Trigger and Echo) . In these 2 pins the output voltage will be only 5V. Whether i can interface these pins with controller? Will it work?

0 项奖励
回复

1,776 次查看
soledad
NXP Employee
NXP Employee

On the LPC178x/7x, I/O pads are powered by VDD(3V3), this is the power supply voltage for I/O other than pins in the VBAT domain; while VDD(REG)(3V3) powers the on-chip voltage regulator which in turn provides power to the CPU and most of the peripherals.

The digital inputs are 5 V tolerant  (5 V tolerant if VDD(3V3) present; if VDD(3V3) not present, do not exceed 3.6 V) providing digital I/O functions with TTL levels and hysteresis.

For digital inputs you can handler 5v without issues, however for digital outputs the maximun output voltage is VDD(3V3).

Please consider that 3.3v is already a HIGH for TTL input pins, please check the below link you can find a conexion that you can use as reference:

Interfacing HC-SR04 Ultrasonic Distance Sensor with LPC2148 


Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,776 次查看
soledad
NXP Employee
NXP Employee

Hi,

For general purpose digital input/output pins the input voltage tolerance is 5v only if VDD>=2.4v 

if VDD<2.4v then the input voltage tolerance is 3.6v.

I hope this clarifies.


Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,776 次查看
mano_hw
Contributor I

Hi

What is the 2.4V means. Is that the controller input voltage or the reference voltage?

I have a ultrasonic sensor which will work on the input voltage of 5V. We have two pins(Trigger and Echo) . In these 2 pins the output voltage will be only 5V. Whether i can interface these pins with controller? Will it work?

0 项奖励
回复