NGX Xplorer Board Internal Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NGX Xplorer Board Internal Flash

885 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cto4260 on Thu Aug 06 01:13:24 MST 2015
Hey everybody,

i want to flash code to the LPC 4300 on the NGX Xplorer board with an LPC-Link2 and LPCXpresso via JTAG.
Everything wents fine and the code excecutes while the debug session.

When I reconnect the device, the code will not be excecuted. I have to flash the board again, to excecute this code.

Has anyone a solution how to excecute the code imedieltly after powring up the board?
It is very important for me to have a solution in the next few days... I hope you can help me.

thanks,
Marvin
标签 (1)
0 项奖励
回复
2 回复数

872 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 06 01:25:41 MST 2015
See this FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/lpc18-lpc43-spifi-flash-drivers
0 项奖励
回复

872 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cto4260 on Thu Aug 06 01:23:59 MST 2015
Okay,
i just read, that the Chip hasn't any internal flash. But the board has an Quad SPI flash.

Can anyone explain me, how to use the SPI flash?
0 项奖励
回复