NFC in phones

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC in phones

Jump to solution
1,136 Views
ujwal_kumar_N_L
Contributor III

Hi community 

I'm working on NFC  RC663 ,i have tried reading NFC tags and cards .Im unable to use phone as a card emulator. The NFC id  keeps on changing as the NFC in phones is used for contactless paying .Is there anyway in which i can use some mobile application and make sure the phone send the same id all the time?
Application is that phone acts as a method of accessing the door system .So i need the ID to be constant .

Thank you and regards 
UJWAL

0 Kudos
Reply
1 Solution
1,123 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

View solution in original post

0 Kudos
Reply
1 Reply
1,124 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

0 Kudos
Reply