NAND-flash and LPC1857

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NAND-flash and LPC1857

742 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by WOVAN on Fri Jul 11 05:05:35 MST 2014
Hi,

i'm designing a datalogger with the LPC1857. I need 1Gbyte of logmemory. i see the lpc 1857 can't address this amount so i'm looking into a  NAND flash. But it is unclear to me if the EMC of the LPC1857 can work with a NAND-flash. and if so, are there any design examples available?

kind regards,

Wouter
标签 (1)
0 项奖励
回复
1 回复

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Fri Jul 11 06:52:18 MST 2014
You should be able to add NAND flash to the EMC.
But: you need a complex piece of software to access the NAND flash!
My advice: don't do that!

Instead: use a microSD card. No pain, you can adjust the storage size by requirement, you can change the card and put it into your PC.

If you want a non-replaceable solution, try a emmc.

regards
Wolfgang

0 项奖励
回复