Moving LPC2366 Keil project over to MCUXpresso? Where is the SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Moving LPC2366 Keil project over to MCUXpresso? Where is the SDK?

1,549 Views
njbuch
Contributor I

I have installed MCUXpresso, hoping for the option of installing support for LPC2366/LPC2368 so I could get started porting the project. But I cannot seem to find any support for this. 

I checked the newest MCUXpressoIDE_10.2.0_759

Any hints and pointers are appreciated!

Thanks

0 Kudos
Reply
2 Replies

1,382 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Niels,

Unfortunately  MCUExpresso does not support LPC2xxx family neither LPC3xxx since these are legacy products only LPCExpresso, IAR and Keil,   suppor this family devices.  I apologize for the inconvenience.

Best Regards,

TIC Support Team

0 Kudos
Reply

1,382 Views
jon_busenkell
Contributor I

Hello jamesbone,

Help! I am porting an LPC2368 project from Keil to LPCXpresso. I have downloaded the latest version of LPCXpresso,

LPCXpresso v8.2.2 [Build 650] [2016-09-09] 

I was hoping that the LPCXpressor environment would come with the SDK (files like lpc23xx.h, and  core_arm7.h) but they do not appear to be included. Can the SDK (header files and specific MCU source files) be downloaded separately? For instance ST has STCUBE/MDK parlance to describe their board level infrastructure.

Thanks in advance for your help. It is GREATLY appreciated.

Jon

0 Kudos
Reply