Moving LPC2366 Keil project over to MCUXpresso? Where is the SDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Moving LPC2366 Keil project over to MCUXpresso? Where is the SDK?

1,361件の閲覧回数
njbuch
Contributor I

I have installed MCUXpresso, hoping for the option of installing support for LPC2366/LPC2368 so I could get started porting the project. But I cannot seem to find any support for this. 

I checked the newest MCUXpressoIDE_10.2.0_759

Any hints and pointers are appreciated!

Thanks

0 件の賞賛
返信
2 返答(返信)

1,194件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Niels,

Unfortunately  MCUExpresso does not support LPC2xxx family neither LPC3xxx since these are legacy products only LPCExpresso, IAR and Keil,   suppor this family devices.  I apologize for the inconvenience.

Best Regards,

TIC Support Team

0 件の賞賛
返信

1,194件の閲覧回数
jon_busenkell
Contributor I

Hello jamesbone,

Help! I am porting an LPC2368 project from Keil to LPCXpresso. I have downloaded the latest version of LPCXpresso,

LPCXpresso v8.2.2 [Build 650] [2016-09-09] 

I was hoping that the LPCXpressor environment would come with the SDK (files like lpc23xx.h, and  core_arm7.h) but they do not appear to be included. Can the SDK (header files and specific MCU source files) be downloaded separately? For instance ST has STCUBE/MDK parlance to describe their board level infrastructure.

Thanks in advance for your help. It is GREATLY appreciated.

Jon

0 件の賞賛
返信