Mistakes in User manual Rev 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mistakes in User manual Rev 2.0

1,880件の閲覧回数
hlsamts
Contributor III

Hereby I would like to start collecting mistaked in the UM10912 users manual. Here is the first one:

Chapter 35.7.11.1 (Initializing DMA), Step 9, see corrections in red:

Start the receive and transmit DMAs by setting SR (bit 0) of the
DMA_CH0_RX_CTRL, DMA_CH1_RX_CTRL and ST (bit 0) of the
DMA_CH0_TX_CTRL, DMA_CH1_TX_CTRL register.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,629件の閲覧回数
hlsamts
Contributor III

And another one:

Chapter 35.7.11.5 (Stopping Starting transmission), see corrections in red:

4. Disable the receive DMA, after making sure that the data in the Rx FIFO is transferred
to the system memory (by reading the appropriate bits of MTL RxQ0 debug register
Table 834, PRXQ=0 and RXQSTS=00).

0 件の賞賛
返信

1,629件の閲覧回数
hlsamts
Contributor III

And here I already found another issue:

https://community.nxp.com/thread/458923 

0 件の賞賛
返信

1,629件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Holger Sachs,

Thanks for your reporting,

I'll check these document issues one by one.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信