Missing information in LPC55S1x datasheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing information in LPC55S1x datasheet

ソリューションへジャンプ
606件の閲覧回数
alexis_marquet
Contributor II

The datasheet for the LPC55S1x does not include information abot termination of DCDC related pins in case the DCDC block is not used.

I think it should be in the "6.1.2 Using the Internal DC-DC converter" but no text is included in this section, only a figure of how to use the DCDC block.

 

 

Best regards,

 

Alexis Marquet

 

ラベル(1)
0 件の賞賛
1 解決策
588件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @alexis_marquet 

As you mention, there is not much information about the related pins when this block is not used, but this is because we do not recommend avoiding this feature. In any case, you could refer to this community post for more information about bypassing the DC-DC converter on a similar LPC: https://community.nxp.com/t5/LPC-Microcontrollers/Properly-bypassing-LPC5500-s-internal-DCDC-convert...

 

Best regards,

Edwin.

元の投稿で解決策を見る

0 件の賞賛
1 返信
589件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @alexis_marquet 

As you mention, there is not much information about the related pins when this block is not used, but this is because we do not recommend avoiding this feature. In any case, you could refer to this community post for more information about bypassing the DC-DC converter on a similar LPC: https://community.nxp.com/t5/LPC-Microcontrollers/Properly-bypassing-LPC5500-s-internal-DCDC-convert...

 

Best regards,

Edwin.

0 件の賞賛