Memory resources used for boot loader for LPC54606

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Memory resources used for boot loader for LPC54606

856 次查看
Jetcitycowboy
NXP Employee
NXP Employee

I also have a separate but related question around the internal flash programming. Is the only way to program/erase the internal flash, from the user application code or the IAR flash writer’s monitor code, by calling the IAP (boot rom) flash programming APIs? If so, can you please clarify on the amount of SRAM0 these boot ROM/IAP can use? 41.3.8.2 is troubling. If the internal boot rom/IAP calls require access to the SRAM0 (or other memory/shared resources) then Microsoft needs to have a list of all such usages, for their secondary boot loader.   If their application needs to call the IAP APIs then they would need to budget resources accordingly.  Thank you.

0 项奖励
回复
1 回复

748 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi ,

Please check my feedback at the thread below:

https://community.nxp.com/thread/449736 

best regards,

Hui

0 项奖励
回复